I am looking for the output voltage of the INA282 when no current is flowing through the Rsense resistor. Can someone point me to that parameter in the datasheet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for the output voltage of the INA282 when no current is flowing through the Rsense resistor. Can someone point me to that parameter in the datasheet?
Hi Steve,
What voltage are REF1 and REF2 at?
For the typical INA282 application with Vout=(1/2)*V+ for Isense=0A:
REF2=V+
REF1=GND
Vo= (Isense*Rsense*50)+(1/2)*V+
Isense=(Vo-(1/2)*V+)/(Rsense*50) This is for current flowing from IN+ to IN- through the shunt.
Example:
Isense=0A
REF2=+5V
REF1=GND
V+=+5V
Vo=+2.5V
Regards,
Jamieson Wardall
Sensing Applications