Hi,
my situation:
SMPS, switching frequency <120khz, Vin <30V, Ipeak 17A, I Need a current Monitor for current mode Regulation, so 17A ==> 1.3V.
Which chip fits?
Thanks a lot.
With best regards
Gerhard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gerhard,
Thanks for your question, we'll review your requirements and make some suggestions Tuesday.
Best regards,
Jason Bridgmon
Hello Gerhard,
The INA168 and INA195 I think will be the best fit.
Regards,
Jamieson Wardall
Hi Jamieson,
INA168 .. 800kHz GBW so with G=10 I am down at 80kHz. f Switch is 75kHz and so I think this is quite too low. As the Peak current is 17A, I have to use a small resistor.
INA 195, GBW also too small and I also Need a seperate supply (Vcc max 18V).
I Need the sensor for Peak current control Loop, so the shape of the inductor current has to be reproduced correct!!!
I ended up with INA139, 4MHz GBW, supply as high as 36V, I have 30V max. I do some Simulation and it Looks fine. Only drawback I have to Limit the gain of the INA139 and use an OP amp to amplifiy the Signal to the needed Level.
Is there a simpler solution?
With best regards
Gerhard
Hi Gerhard,
For a component level power supply I think this is the simplest design for the switching frequency you desire. This the highest GBW solution. You are correct, having 10x the switching frequency to catch the peak current.
Regards,
Jamieson Wardall