Hi Team,
Please let me ask you about the shunt voltage reading of INA219.
Our customer designed a board using this device to monitor the load current. Shunt resistor value is 0.002 ohm.
When they read the shunt voltage with no current flow, it reads out 29h which is 0.41mV.
When they read the shunt voltage with 1A current, it reads out F9h which is 2.49mV.
It seems that the device reading has an offset of 29h and if you subtract 29h form F9h, it is D0h which is 2.08mV (1.04A).
Here are my questions.
[Q1]
Is this offset due to the trace issue from shunt resistor to INA219 pins?
They do have difference in the measured value for shunt voltage and pin voltage.
[Q2]
I cannot understand why there is an offset when there is no current at the shunt resistor. Could you please explain how this voltage appear ?
Load is physically cut off with a switch and INA219 is placed at the load side.
[Q3]
Could you give us the recommended PCB design information, gerber data ?
I would appreciate it if you could give us the data in PDF format, in case I cannot open the gerber data.
[Q4]
Could you also give us the information If there is anything else what the user would need to take care when using this device ?
Thanks and Best Regards,
Kawai