Hi,
I'd like to use INA226 with high side shunt to measure power delivered to the external load (24V/5A). I should also add output short-circuit protection just in case.
Do you thing I can use alert pin with some logic to turn off additional p-mos switch when shunt voltage reaches the programmed limit? Lets say 10A?
As far as I know the alert pin has latch option so the processor will have time to take some action before enabling it before.