Dear Specialist
My customer is using INA199A1 for customer's product.
He is facing a problem of latch-up due to the ESD.
So he has a question about transient specification.
Could you please advise him?
(1)According to the datasheet P.16(IMPROVING TRANSIENT ROBUSTNESS),
Applications involving large input transients with excessive dV/dt above 2kV per microsecond present at the
device input pins may cause damage to the internal ESD structures on version A devices.
Whether latch-up or not, which is depended on the device.
How is the individual specify and the variation?
Could you tell the percentage, if possible.(for example +/-20%, etc.)
He must explain to end user.
He knows INA199B1 but he couldn't change because it has already been in production.
Best regards,
Shinichi