Hi,
I want to build a current sense circuit with the following configuration.
I sense : -50 mA to 500 mA (bidirectional)
Vcm : +/- 10V
Accuracy : +/-10 uA to +/-100 u A
Any help to identify the right part is appreciated. INA282 seems to be good fit. Does 10 mV full scale mean that it is the minimum voltage required to sense?
Regards,
Ajay