Hi,
I hope someone may be able to help?
We have been using INA214A for about 2 years and have been pleased with the device performance and reliability.
We have recently launched a new product with a slightly different design and have seen a 10% failure on the first batch of 200 PCB's.
The application is a DC current monitor for a caravan / motorhome control system, with this particular sensor monitoring the charging current from a solar panel / regulator.
The INA214A should give a 0V output at 0A, but when the failure occurs we see a permanent 3.4 to 3.6A reading (even with no connection to the shunt resistor). The failure is permanent and does not reset after a power down.
The shunt resistor is 0.002R giving a full-scale range of 0 to 25A with our application working in the range of 0 to 10A, so the above failure equates to the output being stuck at about 0.7V.
Our design is made up of 2 PCB assemblies plugged together, with the shunt resistor on one (power) PCB and the monitoring and micro-controller on the other PCB.
I have pasted our schematic below for reference.
After looking into the problem my initial thoughts are that some form of transient is damaging the device, and that a possible move to INA214B may resolve the problem, but I would really appreciate other peoples views as I am no expert.