Dear all,
I've question with this DRV425 of current sensor. I've read the datasheet given that magnetic field rating is +2mT or -2mT. From the DRV425 Evaluation Module it provides the equation (1) for selected the shunt resistor to calculates the B magnetic field values. If I chosen a shunt resistor which is around 0.06ohm and my Vout is 2.5V based on equation (1), then my maximum magnetic field will be around 0.85T. But for this component magnetic field rating only can be measured 2mT. Will I burn the DRV425 current sensor? Does DRV425 same as hall effect sensor principle? So I just need to place the inductor where near to the DRV425 to measure the magnetic field ? Thanks everyone.
www.ti.com/.../drv425evm
Regards,
John