Hi Team,
The customer wants to use INA3221.
Q1: Is INA3221 able to monitor the power supply voltage and to detect if there is sharp drop at some moment?
Q2: Is it fast enough to capture a sudden sharp drop in voltage?
Q3: As in the user guide, there is no timing information shows on the software interface. But if they need to record the voltage against time, is the timing information available from this design?
Q4: He needs to detect the voltage and the current are as belows. +5V/7A; +24V/2.7A;+12V/2.9MA;+24v/2.7MA. Can INA3221 be OK?