Hello,
TINA-TI simulation results show INA225-Q1's slow edge rate of about 2 V / 25 µs when a resistive load of 1 kΩ is put on its output (OUT pin). Does it suggest it's not a good idea to add an RC LPF with 1-kΩ resistor to INA225-Q1's OUT when the PWM signal frequency is 20 kHz?
What do you recommend to filter a noise out from the PWM signal if that's not a good idea?
Best regards,
Shinichi Yokota