ON THE PART NUMBER INA285AID I WONT TO USE THE PART IN A CURRENT SENSE APPLICATION BUT THE PART IS LIMITED TO THE COMMON MODE RANGE I NEED TO NO IF I CAN ADD INPUT RESISTORS ON BOTH INPUT LIKE ADD 1 MEG OHM AT .025% TOL. SO I CAN SENSE THE CURRENT AT 400 VDC BUS SENSE AND ONE IN THE SOURCE LEAD OF THE POWER MOSFET TO MEASURE THE CURRENT AS WELL ...................
ARE WOULD I USE A H-VOLTAGE DIVIDER TO GET TO THE LETS SAY 50 VDC RANGE AND THAN APPLY THAT TO THE INPUTS OF THE PART TO READ THE CURRENT IN THE HI-SIDE AND JUST USE THE COMMON PART FOR THE SOURCE CURRENT SENSE.......................
LET ME NO THANKS FOR YOUR HELP