Hi, I'm working on a project that requires a current sensor. I am using a microcontroller to drive a DC stepper motor. One of the requirements is for the microcontroller to stop spinning the motor when it finds out the motor is stuck before completing its cycle. Research has indicated the motor's current draw will spike from 0.8amps to 1.3amps momentarily when it cannot continue to spin, I need something that once that spike is detected will send a signal to a data pin on the microcontroller, whose software will stop the spinning once that signal is received. Would an INA301 be able to do this or do you have a product more suitable for this type of application?