Other Parts Discussed in Thread: INA282, , INA301, DRV8305
Can TI lab please confirm (inline) shunt monitor 9.2.1 is possible up to 200v maximum. Is not the inline phase voltage CMM completely isolated from VS supply voltage and output pin 8?
It seems the drop across a inline shunt would never rise more than several hundred millivolt same as low side current monitoring. That said even if a motors phase voltage exceeds 80v there should be no current path into VS/OUT from IN+/- or have I missed something here?
The 80v limit seems realistic for a high side monitor where IN+ might connect to B+ and the entire shunt exists before MOSFET drains. This 80v maximum seems less relative when entire shunt exists inline phase mode. Point is there seems should be no path for shunt drop voltage to enter B+ or visa versa since IN+/- exist above ground or B+ but never encounter both sides at the same time inline with a BLDC.
We have used the INA282 up to 190v supply for low side monitors and now INA240 similar case but have discovered a pesky flyback getting into analog data through low side INA240 monitors.