Hello,
I used five INA271 circuits with 20 mOhm shunts on my board to sense current on five different voltage rails.
Two of the INA271 circuits are working fine. Three of them however, are not. Their are experiencing variable gain. Of the three, works with gain cca 35, second one with cca 40 and the third one with cca 18.
I suspect the issue is in improper layout, schematic-wise, the circuits are same for all the voltage rails.However, the two that are working fine and the one that has gain 18, have traces from the shunt in the top pcb layer. The ones with gain 35 and 40, needed to have the traces coming from the shunt crossed, so they are using vias. I can also measure relatively significant voltage on one of the traces from shunt to INA271, on the amplifier that arent working with proper gain, cca 10-15 mV, which throws the INA271 off.
What is interesting is, that even the amplifiers with improper gain, are still working linearly, in other words their gain is constant.
All five circuits have the same +5 VDC power supply. Kelvin connections are used to connect to shunt resistor pads.
Could anyone help me with find the cause of this behavior?
Thank you