Hello,
I faced with problem of the OVC schematic, based on INA200. This is a typical application, based on design in Figure 29 of DS, see attached schematic. The OVC protection is calculated for 334 mA at 24 V. The problem is that there is a current through the BJT transistor connected to C_OUT when circuit receives OVC conditions and it does not disconnect the load, even the current is much larger than the OVC limit.