Other Parts Discussed in Thread: LM25119
Hello,
I need to measure the voltage from 2S (7.4V) up to 6S (22.2V) LiPO batteries.
I have seen the INA282 but I am not sure if I use that or there are any alternatives that can serve my requirements and can be cheaper.
I also need to measure the current, 120A~160A typical and 200A max. Is there any IT component that can serve me?
Best regards
Javier