This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA168: package size of INA168 and INA168-Q1

Part Number: INA168

Hi Team,

I found INA168 and INA168-Q1 use same package but with different size, INA168 is much bigger than INA168-Q1, is that correct? 

 My customer want to find a device which is totally P2P with INA168-Q1, but non-automotive qualified, can you recommend one?  Thanks.   

  • If you're referring to the INA168 measurements on the front page of the data sheet of 18mm x 18mm, those are wrong. The device is in a sot-23 package, roughly 3mm x 1.6mm (see DBV package drawing at the end of the data sheet). The data sheet is being corrected presently.