This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP8646: Current limiter for linear regulator

Part Number: LMP8646
Other Parts Discussed in Thread: LM27761, LMZ34002, TPS62746, TPS62748, LM43600, TPS561208, TPS62125

Can we use this current limiter for the following power supply requirement?

What is the minimum current it can limit?

Can we use linear regulators for the application?

Is there any specific requirement when choosing regulator with LMP8646?

 

1. VOUT = -3.5V

Vin = 5V

Vout = -3.5V (Negative voltage) +/-5%

 Current limit power up = 10mA 

Steady State current = 5mA

Ripple   =  10mV RMS @ 1MHZ

2. VOUT = +1.8V

Vin = 3V

Vout = +1.8V +/-15%

 Current limit power up = 150mA 

Steady State current = 80mA

Ripple   =  30mV RMS @ 1MHZ

3. VOUT = +6.5V

Vin = 9V

Vout = +6.5V +/-5%

 Current limit power up = 100mA 

Steady State current = 80mA

Ripple   =  10mV RMS @ 1MHZ