I would like to use a filter on the Output of the INA 180 and also the INA 210. The 3db Bandwith should be real small, for example 1 kHz. Therefore Input Filtering is not possible that low while referring to the design guide in the pdf (Cf must be real big). The common mode voltage i have in the circuit is small. As you can see the input filter is not really necessary for me. Thats why i want to know, what high frequencies do have for effects on the INA 180/INA 210. Maybe then i need a minimalistic filter.
Best regards
René