Other Parts Discussed in Thread: INA216, INA231
Hi E2e,
I've been using the INA3221 in a battery powered device and it seems working well with a voltage supply below the specified minimum voltage of +2.7V. I've even tested the device with a supply voltage of 2.3V and it is still working.
I'm wondering if it is a good practice to power the INA3221 with voltage below the specified +2.7V? Is there any drawback?
Note that the chip isn't going to measure voltage above its power supply.
In case its really not a good pratice, is there a product like the INA3221 which is specified with a lower supply voltage.
Thanks in advance for your advice.
Darko