Hi,
Referring to the attached schematic, I'm searching for a solution able to measure (no necessary in a accurate way) the current flowing to (from) the load in order to protect the two mosfet (drived by a gate driver IC).
Here follows the application details:
- battery voltage: from 0V to 60V
- The current could flows from the battery to the load (discharge current) but also from the load to the battery (charge current).
- Current value in normal working mode: 40A in both directions
- Shunt value: to be defined but smaller than 0.5mOHM
-
Here follows the current measure circuit requirements:
- Shall be capable to quickly switch off the gate driver when the current (in both directions) is higher then 100A (+/- 15A)
- Shall work in the worst case of short circuit: this means that SNS_a = 60V and SNS_b=GND (and viceversa)
- The total amount of time since the current become higher than 100A to the switch off signal output : 10us (max)
- The solution could consist of one or more IC (in the case of two or more IC please, if it is possible, send me the schematics)
- Cost optimized solution
Thanks a lot for the support
BR
Paolo