Hello,
I have problem with offset on INA240 amplifier!
I have connected INA240 A2 in the evaluation board and I menasure differential output voltage by a multimeter. With 0 input voltage I measure output voltage 0.6mV more then 25uV in the datasheet!
More, the offset I read is not stable! When I restart the circuit supplay I measure 0.3 mV, a little diffrent Vout! So I can not compensate the initial offsett because it is not stable.
The same problem I have in my PCB.
With the INA240-A2 origenaly present in the evaluation board I do not have this problem, I read 0.1mV offset, more then 25uV but it is stable on every restart of power supply.
I have this problem with the INA240-A2 purchased from Farnell ! (N. lotto: 7686956ML7)
Someone has encountered by same problem?
Thanks,
Simone