I am using the INA219 chip which is connected to an 8-bit 8mhz mcu via i2c.
I am using it to measure the current consumption during a GSM transmission
on a SIM800c modem connected to the same mcu via serial ports. But because my mcu is busy
during the transmission I am not able to record the instantaneous current and the
cumulative power consumed during the transmission. Also, because GSM modems
have high peak transmission bursts I am not even able to detect these bursts.
Can you please suggest a way around these problems?
Will I need another deticatgedMCU connected with the INA219 just to log the current
consumption while the main MCU communicates with the GSM module?