Other Parts Discussed in Thread: INA188,
Hi,
Compared with INA188, the power supply for INA240 is very simple, so I don't think it is a general amplifier. It must have a resistance network at the input to attenuate the input common voltage.
I want to use it in a high side shunt current sensing application. I could use either INA240 or INA188. The offset of INA240 is 25uV, and it is 55uV for INA188. Does it mean offset of INA240 is really smaller than INA188? If their definitions are same(apple to apple), I think INA240 has more advantage with simpler power supply and smaller offset.
Thanks.