I've read TIDUA90 as well as the applications section of the data sheet regarding paralleling 2 INA250 for measuring > 15A.
I would like to put 3 of them in parallel to measure 0-40A.
Rather than daisy chain the outputs as shown in the aforementioned documentation, I would prefer to use a resistor based voltage summing circuit to to get the sum of the outputs.
I imagine that summing the outputs is probably not an issue.
However, I am wondering what the true tolerance of the internal shunts may be- when we start hooking many in parallel, a device having a lower shunt value will "hog" more of the current?
Has anyone analyzed the limit of how many of these things can be hooked in parallel?
Thanks, Best, Steve