• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Amplifiers » /etc... Amplifiers & Other Linear » /etc... Amplifiers & Other Linear Forum » The Best Amplifier for the LM335?
Share
/etc... Amplifiers & Other Linear
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

The Best Amplifier for the LM335?

This question is not answered
Tsion Addisu
Posted by Tsion Addisu
on Apr 27 2012 18:55 PM
Prodigy20 points

I am making a simple circuit that uses the LM335 precision temperature sensor, and the output voltage signal I am receiving from this device has an extremely small range (2.92 - 3.04 V). I want to find an operational amplifier to widen this range to 0 - 5V, but I don't know which op-amp to get. Which op-amp should I buy for my requirements on the LM335?

LM335 LM335AZ Op-Amp operational amplifier
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Thomas Kuehl
    Posted by Thomas Kuehl
    on Apr 30 2012 17:45 PM
    Mastermind24240 points

    Hello Tsion,

    The output from your LM335 is centered about 2.98 V and would move over the 12 mV over the span you listed. There is the large dc component amongst the temperature-related level change that an amplifier following the LM335 must handle. Then, you need a large dc gain of approximately 417 V/V to amplify the 12 mV change, to a 0 to 5 V change. That 0 to 5 V range then needs to be level shifted to achieve the 0 to 5 V output level you want.

    My suggestion is to use a instrumentation amplifier for the amplifier that follows the LM335. The CMOS INA333 instrumentation amplifier would be very suitable for this task. You would need a stable reference voltage of approximately 2.92 V  and this would be applied to the inverting input of the INA333. The LM335 output would be applied to the non-inverting input. The INA333 gain would be set to 417 V/V with a ~ 240-Ohm gain-set resistor. The LM337 will amplify the difference between the reference voltage (2.92 V) and the output of the LM335 and amplify it by 417 V/V. However, the resulting 0 to 5 V change has to be centered about 2.5 V to achieve the 0 to 5 V output. The 2.5 V would be applied to the INA333 reference pin. So the circuit requires two accurate reference voltage; 2.92 V and 2.50 V.

    No amplifier can swing fully to the power supply levels. The INA333 can swing to within about 50 mV of the power supply rail when driving a 10 k-Ohm load. Increasing the resistive load will allow it to swing even closer. If you increase the power supply to +5.25 V, or +5.5V, then the output will swing all the way to 5.0 V. The low end will still be limited to about 50 mV above 0 V. To truly swing 0 to 5 V a dual supply (+/-15 V) instrument amplifier such as the INA118 would be required.

    I hope this helps you get on track with your design.

    Regards, Thomas

    PA - Linear Applications Engineering

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tsion Addisu
    Posted by Tsion Addisu
    on Apr 30 2012 21:27 PM
    Prodigy20 points

    Ok. I am building the circuit on a Dragon-12 USB evaluation board, which has a 5 V power supply that feeds into the circuit. This is for a college project.

    So, to summarize what you said: all I need to do is input the resulting voltage from the LM335 into the INA333 through its non-inverting input. Is the LM337 required as well to properly amplify the voltage?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Thomas Kuehl
    Posted by Thomas Kuehl
    on May 02 2012 11:32 AM
    Mastermind24240 points

     Hi Tsion,

    We had some E2E forum problems yesterday and I was able to post my response until now. Sorry for any delay.

    The LM337 is a negative voltage regulator and I don’t think you will need it for your circuit. It is best for this application to avoid using a 3-terminal regulator as the reference. Although great for general supply regulator purposes most often they are not precision devices.

    I gave your application a little more thought and all that it requires is the 2.92 V reference voltage applied to the INA333 inverting input pin. Then the output of the LM335 would be applied to the INA333 non-inverting input. The 2.5 V reference I mentioned in my previous post is not needed.

    About the easiest way to attain an accurate reference voltage is to use a voltage reference IC. I suggest the REF5030 to generate the 2.92 V input level. Although the REF5030 is a 3.0 V reference, it has a Vout adjust pin that allows the actual output voltage level to be adjusted about 15 mV above and below the internal 3.0 V level. Figure 24 in the data sheet shows how this function is utilized. The adjustment will allow you to accurately set the 2.92 V input level and be used to compensate for other offsets in the system.

    Regards, Thomas

    PA – Linear Applications Engineering

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use