This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMV324: issue with lmv324 buffer output limits to 2.7v

Part Number: LMV324

HI ,

iam using LMV324ID AS a buffer ,

VCC 3.3V, but out of the buffer is latching to 2.71 to max of 2.74.  even my buffer input crossing 3V.. why ? any limitation in the part ? i am expecting buffer out put should follow the input .

Please help me .

  • Hello,

    In a buffer configuration the input common mode voltage is equal to the input voltage. The input common mode voltage of the LMV324 is specified 800mV (typical) from the supply rail. Therefore, when the input goes above 2.5V on a 3.3V supply the LMV324 is no longer in a linear operating region. For more information please see our TI Precision Lab videos on input and output limitations.

    Thank you,

    Tim Claycomb

  • In reply to Timothy Claycomb:

    Both curves are normal behavior.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.