This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2901: Frequency to Voltage conversion

Part Number: LM2901

Hi,

I need to design a signal conditioning board for a tachometer generator input. The input will be 3 Phase AC with variable frequency of 0 to 80Hz and amplitude 10V  ( in each line).

As the motor RPM changes, frequency changes. Please suggest me a frequency to voltage converter IC for sensing the frequency change.

Thanks & Regards,

Madhu.

1 Reply

  • Hello Madu,

    See the datasheet for the LM2907/LM2917 voltage-to-frequency converter:

    There is an applications note that may prove helpful:

    Regards, Thomas

    Precision Amplifiers Applications Engineering

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.