Hi,
I am using DAC0800 which is giving a negative voltage. I tried to convert it to positive by using inverting amplifier but the voltage is getting decrease like if am getting 0v for min. input of DAC and -5V for max. input of DAC after converting 1.9V for min. DAC input and 5V for max. DAC input. Is it possible to get a 0V for min. input of DAC after converting?
This is our first project.Please do help.