What kind of magnetic sensor works with the LM2907 input. 2 wire magnetic pickup, or 3 wire hall effect NPN open collector or? Can you draw a diagram? Shaft speed in this tachometer circuit is 0 to 7000 RPM. What is the formula for Hz with the known components of RPM and number of teeth or magnetic pick up points . Can there be just 1 pick up point or can there be 6 or 8? We can install a plate with holes in it, for magnetic sensor target. or we can install a plate with magnets for a sensor target. What would you reccomend here?
Thank you
Dean