Hi,
I have six 3.6V battery cells in parallel going into a TPS63000. Each battery is in series with a diode and a 250mA fuse. All the cells combine and an 80mA master fuse is then in series. The 80mA fuse has a resistance of ~8 Ohm. Without this fuse the whole circuit works fine. I reckon the fuse resistance is showing a lower voltage and the TPS struggles to power up. I reckon, using an op-amp with very low output impedance (<1 Ohm) as a buffer before the TPS buck boost might solve the problem (V+=Vin+ = 3.6V, Vin- = Vout, V- = GND). Any thoughts are welcome on this.
If this is a viable solution, which op amp should I use? The voltage output og the TPS need to be 3.3V and utilise the battery as much as possible (may be down to 2.0V?). The max current that will be drawn by the load will be about 65 mA.
Thanks
Chris