There is severe output offset voltage when using the design according to the Application Bulletin; SBFA005 / AB-062; "Digitally Programmable Time-continous Active Filter".
When setting low cut-off frequency, an offset voltage will appear. The lower set frequency, the bigger offset. The offset voltage is negligible for frequencys above 15-20Hz, but will increase dramaticly under 10Hz. The cut-off frequency in this design can in theory be set as low as 1Hz. But under 3Hz is impossible to use the design. From 3Hz it's possible, if the right type of amplifier is chosen and manual offset trimming of the amp's is added. OPA627 will not work. OP37 has previous been able to use.
I would be very glad for any input!