Hi,
I need a sine wave ac constant current source. I need to synchronize the sinewave to another part, so I create the sine wave using a dac.
Freq is around 800 Hz, fixed. And load resistance is between 1Kohm to 1 Ohm. The system will be power up with +/- 12V rail. So, current is about 10mA.
Any suggestion on the current source circuit ?
Thank you so much.