Hello,
I currently have my LM8358 connected the way it is in Figure 61 on page 32 of the LM8358 datasheet. This would make it so that the bias reading I get from this amp to 2.5V. I'm trying to run the diagnostic in which i send the AMP 0x0082, meaning that I want to set the MUX in the configuration where I ground IN- and attenuate IN+ by 50 and set the gain setting to 50. When I take this reading, I get 4.993377 V. Because of the Reference Bias, I subtract 2.5 V from this to get around 2.5V. However, let's say that the IN+ is shorted to V+. Theoretically, it would be 7.5V due to the Reference Bias but the chip is unable to send out a voltage over 5V. What configuration would I need to do in order to determine whether or not the IN+ is shorted or working properly? Thank you.