it is my understanding that the input referred noise current (density) can be obtained from Ibias via
inoise=sqrt(2*q*Ibias), where q=1.6e-19.
on the datasheet for the OP365, both Ib and the input referred noise current are specified. When I plug the Ibias from the datasheet into the equation above, I do not get same shown on the datasheet for Inoise.
ie, Ibias=10pA.
inoise (calculated)=sqrt(2*q*Ibias)=1.7fA/sqrt(Hz).
the datasheet shows 4fA/sqrt(Hz). Why the difference?
Thanks!