Hi everyone.
Here is the testing condition.
+VS1=12V,GND1 connect to -VS1.
+VS2=12V,GND2 connect to -VS2.
And what I input to Vin is a 2.5V DC offset with 200mV(1kHz) sinusoidal wave.
However, the Vout is pull high and it seem that Vout regardless of Vin, even though I pull down the Vin to GND1, the Vout still high.
I had changed another ISO124, but it still can't work. So i think the circuit configuration might be wrong.
Does anyone have some strategy for it?
thx a lot.