Hello
ISO122 input offset voltage is +/- 50mV max at Vs1=Vs2= +/- 15V .
Even though Vs1=Vs2= +/- 5V, is offset voltage same ? Or, becomes bigger?
Cusotmer use as Input voltage is 0~2.41Vdc.
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
ISO122 input offset voltage is +/- 50mV max at Vs1=Vs2= +/- 15V .
Even though Vs1=Vs2= +/- 5V, is offset voltage same ? Or, becomes bigger?
Cusotmer use as Input voltage is 0~2.41Vdc.
Best Regards
Hello Kanji Shibatani,
Unfortunately we do not have characterization data for power supply conditions other than those specified in the ISO122 datasheet.
Best regards,
Jose