I'm using OPA 2336(~4V single supply) w/unipolar positive signals few mW above ground successfully but need to use for ~100mV BIPOLAR inputs and have no space for dc-dc. I have used other single supplies w/limited(~100mV) bipolar input by adding a forward bias schottky(~200mV FVD) to the opamp ground. but the 2336 doesn't like it it saturates ~25mV above ground and I need to measure 0.000mv or negative signals