Hi All
I implemented four voltage follwer with TLV2374.
The two voltage follower is Reference voltage for NTC thermister.
And the others is NTC Thermister voltage divider buffer.
I saw the instability of voltage followerr output. But, I can't duplicated it so far.
I have question about the TLV2374 internal compensation function.
I added 100nF Capacitive and 10K in-line resistor to predict the voltage follower oscillation.
Does the TLS2374 has internal compensation circuit?
also, The TLS2374 might have an instability condotion at voltage follwer???
Please let me know.
Thanks
Ethan