The schematic is similar to http://www.ti.com/lit/df/tidr225/tidr225.pdf .
3 temperature :-20,25,70
When my sensor's offset ≤±5mV/V and span =20mV/V ,after calibrated ,the result is well.4mA and 20mA output error bouth ≤0.2%FS when the temperature is -20,25,70 .
But my sensor's offset ≤±5mV/V and span =30mV/V ,after calibrated ,4mA output error is well.20mA output error is close to 0.5%FS(19.920mA) when tempreture is 25.if I only write one tempreture(-20 or 25 or 70) data to EEPROM,the output is well(error ≤0.1%FS,-0.016mA~+0.016mA) when the product in Corresponding tempreature.
I try to use 4 tempreature(-20,0,25,70 or -20,25,50,70) to calibrate my product,but the result is same:20mA output error is close to 0.5%FS(19.920mA) when tempreture is 25.
Please give me some suggestion,thank you.
Best regards.