I have a DAQ in the test equipment which must remain within ~11V of test inputs. The test equipment ground and the product ground are connected via a cable, but if I connect them directly to the AI Ground of my DAQ, differential readings will be impaired (due to load imbalance). I want to generate a virtual ground for the AI Ground from the Product ground. I am using OPA548's to create a High Current amplifier already in my Test Equipment. Is the OPA548 suitable for use as generating the Virtual Ground input for my DAQ?
My greatest concern is that all my power is Single Ended, positive suppies only, and how effective will the Virtual ground be if the output is nominally at V-, or 0v in this case? What will negative noise due, for instance?