Hello,
I am trying to build an 8 cylinder, breaker point automotive tachometer based on info of document SNAS555C, page11. My goal was to have 2.5 VDC output at max 533Hz. I have wired it for the input at pin 1 and 11 as the document shows using the exact values of components shown. I used 0.02uF at pin 2. 31K ohm // to 1.0uF at pins 3 with 4.
It all seems to work as expected at frequencies below about 400Hz, but much above that, the output voltage measured at pins3,4 decreases.
V should be 7.56 x.02E-6 x 31E3 x 533Hz = 2.498
I don't know what I'm missing and any help would be much appreciated!
Thanks