Hi analog expert,
1.In TI application report(reportNo:SLOA059), in page 3, the description to input offset value(Vio) is as below :It can be either negative or positive in polarity;
2.In TL072A datasheet, page6, the parameter Vio: input offset value has the max value :7.5mV in full range.
3.So my question is : just a +7.5mV is listed in the table, What's the negative limit value for this parameter about the PART TL072AC? Or the 7.5mV means the input offset value is within +/-7.5mV ?]
TL072A max Vio 7.5mv has been listed in table try to illustrate positive polarity characteristic only ,??
according to some other amplifiers datasheet like OPA277,max value ±20mv has been listed in table for demonstrating the Bipolar polarity and the figure “OFFSET VOLTAGE PRODUCTION DISTRIBUTION” in page 6 has also descripted this spec, 2 ways for descripting VIO which have same explaining ??