Hi,
I use an AMC110 and lost the second device now. Is there any power sequence needed? As I power the low side with 3V3 from an EVAL board, the 3V3 supply is still there if I power of the rest of my circuit and so the hi side of the AMC110.
Any suggestions how to power the AMC1100 correct?
When hi side is off, I see my small negative bias of 0.23V (LM7705) at the Output, Problem? After power on the hi side I get 2.55V but Input is Zero, so something must be wrong.
The first device died and than the chip gets very hot and draws lot of current at the hi side. Low side seems to be ok.
No, there is no high voltage around, 180V max.
Thanks for helping.
With best regards
Gerhard