Hello,
I had a question about clipping of a 60 Hz AC signal when it is passing through an LM324. The LM324 is biased with 12V and DC and the input has a virtual ground at 1.65V. The gain of the op-amp is such that the output signal will swing between 0V and 3.3V. In real life, this signal is swinging between 640mV and 3.3V.
However, when I replace the LM324 with TLC274 the output swings very cleanly from 0V to 3.3V. This setup is on a breadboard, and no other change is made except pulling out the LM324 and putting in the TLC274.
The signal is from a function generator with the intention of figuring out that a barebones op-amp like the LM324 would work for my application. I do understand that the LM324 has higher offset voltage and poorer CMRR, but I am not sure how that would cause this issue.
Thanks