This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

which op amp to use - low voltage (USB) xr 4136 replacement

Other Parts Discussed in Thread: OPA2334

Hi, I understand that this is an egineer forum (and I am just a beginner no egineer) but the problem is that I probably cannot google correct question at google , so I appologise for very basic question in advance.

My idea is to replace xr 4136 in below mentioned circuit with op amp that could be USB powered +5V, single supply.

Could you suggest me some suitable replacement if that is possible? It is basically guitar preamp with line mixer to it. Would LMV797B or OPA2334 do any good?

Thank you very much

Michal