Please help.
I have designed a discrete power switch as in the attached TINA simulation model.
What I expect is:
When VG1 is high (5V), VF3 is low and VF4 is high and the output should be +5V instead of +12V.
But the simulation result is wrong as below:
when VF3=low and VF4= high, why T1 is conducted and the output1 is showing +12v?
Please help me to find the reason for this, many thanks.
David.