This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Moha,
Please use a rich formatting option on the bottom to Insert/Edit Media - we cannot see schematics that were pasted into the body of the forum post and without it it is difficult to address your question.
Having said that, please make sure you meet the minimum 2.5V supply requirement (see PDS table below) plus the voltage drop across the resistor used; in case of using 50k resistor together with 100uA constant current source, you need a minimum of 7.5V voltage supply (2.5V+100uA*50k).
Moha,
Are you certain the buffer is faulty? Reading the input voltage at pin 3 with a standard meter (10M ohms) will lower the voltage at pin 3. If the same meter was used to measure pin 1 later, the voltage at pin 1 will be higher because pin 3 is not loaded with the meter anymore.
You may measure the voltage between pins 1 and 3 to see the error.
To use TL084 the -15V supply should be increased to -4V to cover the input common mode range for TL084.