Hi,
In an application I'm required to generate a 2MHz 3.3V CMOS square wave clock from a sine wave of the same frequency. I was considering using TL3016ID ultra fast precision comparator for this application, by setting VCC+, VCC- as +3.3V and -3.3V respectively. Can you please say if it is fine, can I expect to obtain 3.3V CMOS levels at the output with these supplies?
Also, I understand that all the specifications provided in the datasheet are for +/-5V supplies, is the performance expected to suffer significantly if I use +/-3.3V supplies, especially in terms of jitter, rise/fall time etc?
Plus, can you comment on the internal hysteresis specification for this part, how much input noise can it tolerate without resulting in faulty switching?
Thanks,
Anoop