Hello Folks,
My application is a precision low current source where I need to generate current as low as 1nA and maximum of 100uA. This would be used to test my analog input circuit which interfaces to a amperometric sensor.
I plan to use the circuit (b) shown in the datasheet of REF200 page 9 wherein I can generate current of 1nA. This circuit recommends the use of OPA128 opamp. I have done a POC (Proof of concept) using samples from TI and it works fine apart from the noise that is obviously present due to noisy power supplies and lack of shielding during POC.
The OPA128 uses a dual +/-15V supply and it very costly, somewhere around USD 40. I was thinking of using a cheaper precision opamp like LMP7721 instead of OPA128. The only problem is that LMP7721 and most other precision opamps use a supply of 5V.
My question is that if I replace OPA128 with LMP7721, will there be any issues with the circuit operation? As per the REF200 datasheet the compliance voltage range is 2.5V to 40V, so the 5V supply should work. Am I right?
Regards
Nikhil